Use this process to convert a Google Earth kml file to an NMEA GGA file for use by the scenario generator.
If playing a scenario, click the button.
In the tree node, click the node.
Click on the to launch the dialog box.
On the dialog box:
Click to launch the dialog box to navigate to and open the saved Google Earth kml file.
After selecting the kml file, the file path and name appears to the right of the button..
If desired, change the file properties for the conversion.
Click the button to launch the dialog box for selecting a location and saving the file as an NMEA GGA file type.
After saving the converted NMEA GGA file, click the
to close the dialog box.
Click the node.
Click the cell and use the drop-down arrow to select .
With the selection, the cell appears .
Click the cell, and use the dialog box button
to launch the dialog box for navigating
to and selecting the converted NMEA message file.
After selecting the file, the cell automatically updates to the start time from the GGA file.
The start time in the scenario generator uses GPS time versus UTC time for the Start Time property of the KML to NMEA Converter. Because of the different time types, the scenario generator start time will always show a number of leap seconds later than the KML to NMEA Converter, Start Time property.
Change the date of the cell to match the date of the almanac file.
For the factory supplied almanac files, the date is part of the file name or you can view these almanac file dates in the Factory Supplied GNSS Files topic.